The App Home + Security works also on tablet. When in landscape position, conceived for optimal video viewing, it is not possible to use answer/end call and open lock buttons. Just place the tablet again in vertical position to show and use the buttons.
You will find the installation instruction of your product in its packaging. Otherwise, it is available on the web catalogue page of Smarther with Netatmo connected thermostat (http://www.homesystems-legrandgroup.com). For further installation details, you can watch the tutorial https://www.youtube.com/watch?v=FVZF83c2NWM&list=PLR4fOw5f1yqQE4-z0RLsAwy5SJK7x4u7s&index=2
The algorithm is your connected thermostat's 'brain' and allows it to make decisions and fire up the boiler based on: heating history, room temperature, setpoint temperature and the chosen heating algorithm.You can switch between the Hysteresis and PID advanced algorithm in the app settings: Settings > My Home > Room of your thermostat > My thermostat > Advanced settings.Hysteresis algorithmWith this algorithm, when the difference between the setpoint and room temperatures is within a given sensitivity threshold, the thermostat assumes the setpoint temperature has been reached.You can adjust the Hysteresis algorithm sensitivity threshold in the thermostat's advanced settings. If you use smaller thresholds (0.1 °C), the thermostat will be more responsive to room and setpoint temperature changes. With larger thresholds, the thermostat will be more tolerant to variations in these temperatures and will switch the heating on and off less often.NB: This algorithm is recommended for wood-burning stoves.Advanced algorithm (PID)The Proportional-Integral-Derivative (PID) heating algorithm is more intelligent than the Hysteresis algorithm, enabling improved temperature regulation with fewer oscillations around the setpoint temperature. It takes the specific characteristics of your home into account (thermal inertia, insulation, etc.).When you first install the thermostat, only the Hysteresis mode is available.Over the first few weeks of heating, the thermostat will determine the specific characteristics of your home, including its thermal inertia and insulation.The PID cannot be activated until the thermostat has completed this initial configuration.It can then be deactivated to switch back to Hysteresis mode.Comments • Settings can only be configured during cold periods, when the Thermostat is actively controlling the heating. • When the temperature in the home rises quickly, you are advised to use setpoint temperatures with several degrees' difference between Comfort mode and Eco mode to give the thermostat clear benchmarks. Specific issues • The advanced heating algorithm (PID) is only useful for systems with high inertia, and is therefore not recommended in cases where the standard Hysteresis algorithm is already producing excellent results (heated floors, etc.). • The advanced heating algorithm is not recommended for devices that require significant fire-up and shut-down times since this can adversely affect their good working order and lifespan (examples include pellet-fired stoves and some heat pumps). • The PID is automatically deactivated for all setpoint temperatures up to 14°C; there is no point in using the heating more often to turn it on or off when nobody is home. • For Netatmo Smart Radiator Valves, the system will automatically switch to PID mode once configuration is complete. Neither of the algorithms can be force-activated.
It is possible that your products won't automatically appear in the Home App from Apple at the end of the installation. This may be the case if, for example, the initial installation of the products was done using the account of a friend or family member or with an Android smartphone. Go to the Home + Control application settings and select "Manage my home", select the room in which the thermostat is installed, select the thermostat and " HomeKit & Siri". Follow the instructions in the application to configure the thermostat with HomeKit.
1) Be sure your thermostat is well powered. You should see the temperature on screen.2) Power it off and power it on again. Then try to push the button on the top right side for few seconds to make the "AP" appears on screen. The Wi-Fi sign should also be blinking.3) If it still doesn't work please contact our support team.
To reset Apple HomeKit on your thermostat please follow these steps: Verify that the thermostat is well powered. Press and hold the button on the bottom right side of the product until you hear one beep. Then release the button and wait for the thermostat to reboot.During this procedure, you will see on screen a countdown of 5 seconds.Go to the Home + Control App to reconfigure the Wi-Fi settings which have been reset.Go to settings, select "Manage my home", select the room in which the thermostat is installed, select the thermostat and select "Wi-Fi setup". Then follow the instructions step by step given by the application.
The Home + Control App allows you to control as many homes as you wish from one single account. To control an existing connected installation, you just need to ask an existing user to invite you. Once you are invited in a home, you get the same access rights than the person who invited you.To set up a new installation, just go in your Home + Control App settings and select "Install a new home".
In the event of a power cut, your thermostat will no longer work. However, the product is designed to function again as soon as the power comes back on, and go back to the state they were in before the power cut. Please note that the thermostat can take a few minutes to reconnect to the Internet and be accessible again via the application.If you are cut off from the Internet, your thermostat will still work locally and will follow its schedule. During the outage: You can't control your installation via the Home + Control application or change the settings. You can however control and see the temperature directly on the thermostat. The Home App from Apple remains operational as soon as the local connection to the Router is maintained. You will automatically find all the features as soon as the Internet connection comes back on. Please note that the thermostat may take a few minutes to reconnect.Regarding the Netatmo Smart Radiator Valves, they will continue to work and will follow their schedule during a power cut or an Internet outage. You can also control and see the temperature directly on the valves.
The Home + Control Android application is downloadable from Google Play.Since May 2020, some smartphone models are no longer certified by Google, so they no longer use Google Mobile services and therefore Google Play.The Home + Control application use a set of Google services to function, so they are not compatible with another universe of applications and services. The models for which our application is not compatible are the following:Huawei P40Huawei P40 LiteHuawei P40 Lite 5GHuawei P40 Lite EHuawei P40 Pro+Huawei P40 Pro Huawei Mate 30 ProHuawei Mate 30 Honor 9X ProHonor View 30 ProHonor View 30