You can have 1 up to 10 HOMETOUCHYou could connect all on the same Door Entry System bus maximun 5 HOMETOUCH (each one with it's dedicated power supply)From 6 to 10 HOMETOUCH it's necessary realize a Door Entry System Expansion; for more details read Doo Entry System technical guideOnly one HOMETOUCH must be sincronized to the APP
The thermo area are divided in 2 parts.In the top ones you can find general themo status by edge color border (red heating, blue air conditioning) that at least one of the zones is active, icon for mode set and info about number of active zonesIn the bottom ones you can find info about Favourite thermostat: temperature misured and status by edge color border (red heating, blue air conditioning)
Voice control Alexa is a digital control device with integrated Amazon Alexa voice assistant, including 2 touch controls for lighting managementAlexa is an intelligent personal assistant developed by Amazon that allows voice interaction between you and the Internet, allowing among other things, voice communication with your connected Legrand home.
If you are unable to connect your Voice Control Alexa to the Internet:Turn off the Voice Control Alexa power at the main switch, then turn it back on and restart your Internet/Wi-Fi router. If this does not solve the problem, and if you have already manually configured your router, it may be that the Router's configuration blocks the connection to the Voice Control Alexa. In this case, refer to your router manual and follow the instructions:Step 1: In the Internet browser on your computer, type in the local address of the router, in the following form http://192.168.x.x (e.g. http://192.168.1.1). This is shown in the router manual.Step 2: Sometimes a username and password are requested. With most routers these are "admin" and "admin". Otherwise refer to your manual.Step 3: You can then access your router's configuration interface.Step 4: If you use parental control, check that you have definitely authorised the Voice Control Alexa. To do this, check if its MAC address (see: Where can I find the Voice Control Alexa's MAC address?) is in the list of authorised devices.Step 5: If you use a standby feature for your router, deactivate it.If you are still unable to reconnect, proceed as follows:Step 1: Firstly, try to assign a fixed IP address to the Voice Control Alexa by indicating its MAC address (How do I find the my product's MAC address or serial number?). If you have an Android smartphone, you can also assign a fixed IP to the smartphone.If needed there are tutorials to help you with this configuration: in your browser, type in the brand and model of your router. Then write "static IP for MAC address" in your browser.Step 2: Then, you can check the Wi-Fi frequency band used by your router. The Voice Control Alexa does not work with the frequency 5 GHz. Make sure that the 2.4 GHz mode is activated.Step 3: If the Wi-Fi channel has been modified manually, it may be that it no longer makes an optimal connection possible. Check that the "automatic selection of Wi-Fi channel" mode is activated. Step 4: Finally, if your network is equipped with one or more Wi-Fi repeaters, make sure that each of these Wi-Fi access points has a different name (or SSID) and that the Voice Control Alexa connects to the one which has the strongest signal.
Om uw Alexa-stembediening los te koppelen, moet u ze resetten in de Digital Controls app. Vergeet daarbij niet de Alexa-stembediening te verwijderen uit de lijst met toestellen in de Alexa-app.