Aller au contenu principal
Logo print
As soon as the firmware is released, it will be automatically downloaded on the installation (if the server is connected to internet).
Consulter les questions fréquemment posées
If you have no Internet connection, the manual management of lights, shutters and thermoregulation by local commands still work. Also HOMETOUCH continue to work.All the functions present into MYHOMEServer1 will properly work except online functionalities ( app, push notification,meteo).
Consulter les questions fréquemment posées
Open the hamburger menu, select “Schedules” and then “Action”: here you will find your home actions program, in which will be possible to add the on/off (and fan speed) of these thermo objects, based on time&date.
Consulter les questions fréquemment posées
Scenario is a specific set of actions of the installation like a defined status of lights, shutters, thermo and sound system user can recall manually by local comand, HOMETOUCH, on smartphone by application or even vocal assistance if itegrated with the installation.
Consulter les questions fréquemment posées
Download Home + Control App from Play store or App Store and follow the start up procedure. Select MyHomeServer1 from the product list and insert the user code available on MyHomeServer1 device.
Consulter les questions fréquemment posées
In the event of a power cut, all objects doesn't work like conventional installations. However, as soon as the power comes back on, MYHOMEServer1 replace the status of all objects as they were before (memory function).
Consulter les questions fréquemment posées
Right now, the installation test using Home + Project is not possible: the only way is to configure through H+P and then test what you have done through H+C. Locally, if what you configure is associated to a physical pushbutton, you can test it after the object configuration.
Consulter les questions fréquemment posées
HOME+PROJECT can configures: max 30 rooms, max 50 objects for room.For each object it's possible to link max 50 local pushbuttons/contact interface.
Consulter les questions fréquemment posées
S'abonner à